Search Results for marport extract data
Applications - Marport
Examples of data received and displayed in Scala2 application. 1. Catch status: empty / 2. Catch status: full / 3. The echogram shows the codend filling up, until the catch sensor is triggered. Last updated: December 17, 2024 ...
Connecting the Sensor to Mosa2 - marport.com
The sensor has an automatic range mode that is useful to get better quality echograms when the trawl is close to the bottom.
Airmar aquires Marport
Marport Deep Sea Technologies Inc. was founded in 1997 to develop acoustic monitoring systems for the deep sea commercial fishing fleet and has been a leading innovator in sensor solutions in that sector ever since. Marport’s R&D division will be based in Lorient, France following the acquisition.
Saving a Configuration on Mosa2 - marport.com
Mosa2 has a virtual water-switch option that changes the conditions under which the sensor is running.
Marport
Marport Norge AS Breivika industriveg 69 6018 Ålesund Norway Eng. Tel. 70 23 81 00 . Rev. Monitors and cables are YARD SUPPLY. Marport is delivering five ... linked to same data squid Rev. 25.0219 First issue Date Description VARD Aukra NB-894 Orginator: Verified: J.S G.G Marport Norge AS Breivika industriveg 69 6018 Ålesund Norway
General Installation Instructions and Drawings - marport.com
It is important to carefully plan the setup of your sensors before adding them to the system. You can create a table with a list of frequencies and complete it when you add sensors.
Defining a Hydrophone - marport.com
Refer to List of Marport Hydrophones to learn about Marport different models of hydrophones. Procedure. From the left side of the screen where the system is displayed, click Hydrophones. To add a hydrophone to the system, click Click to Add on one of the hydrophones ports. In the hydrophone selection page, scroll the top part to see the ...
Customer support
This page provides a summary of the latest changes in Marport documentation. The service documentation is available on Marport Authorized Service Provider platform. Product Documentation
Getting Started - Marport
Learn how to connect to the sensor by short-range wireless connection, to be able to connect with Mosa2 and configure the sensor. Mosa2 and configure the sensor.
Main Parts - marport.com
External View 1. Retainer screw 2. Model/serial number 3. Metal strap 4. Transducer 5. Stabilizer board 6. Pressure sensor 7. Temperature sensor 8. Positive charge 9. Negative charge 10. Water switch ...
Installing the Sensor on the Trawl - marport.com
Place the sensor on the center of the net's headrope if it is in Down Looking mode or footrope if in Up Looking mode. The side with arrows must be oriented toward the vessel.
Overview of Scala2 - Marport
1 Menu 6 Incoming Data 2 Toolbar for Page Display 7 Receiver Activity 3 Data Display 8 Echogram Time Stamp 4 Control Panels 9 Alarms 5 Customizing panel (Customize mode only) Back to support page. Jump to main content Scala2. V. 02.14.x Index. Search. Home; Introduction and Presentation ...
Marport - Useful Resources
Scala2 Language Files. Only for Scala2 versions 02.00.00 to 02.08.x. In above versions the language can be selected directly from the application.
Introduction and Presentation - Marport
This is an example of data received from a Trawl Explorer sensor and displayed in Scala2. Safety Guidelines. Read this section before using the product. Description. Installation Steps . Introduction and Presentation. Read this section to get a basic knowledge of your Trawl Explorer sensor.
Frequency Plan - marport.com
Marport Pro sensors (e.g. Trident, Door Explorer, Trawl Navigator, Speed Navigator) Example: If the frequency of the sensor is 40kHz, there should be no sensors between 39.8-40kHz and 40-41.2kHz. Figure 3. NBTE ...
USER MANUAL - Marport
Learn how to configure the receiver to be able to receive and display Door Explorer data. Installation. Learn how to install the sensor on the trawl gear. Maintenance and Troubleshooting. Read this section for troubleshooting and maintenance information. Useful Resources.
Installing Catch Sensors on the Trawl - Marport
Sensors can be installed with the pull cords on the side or on the center of the sensor. Pull cords are attached to the net. When the net fills up and the meshes expand, cords are pulled and this triggers the catch sensor.
ABOUT US - Airmar
In October 2013 Airmar acquired long-time partner and collaborator Marport, which designs and manufactures catch control and net monitoring sensors, echo sounders, current profilers and sonar for the world’s fishing fleet. ... Technical Data Catalog (pdf) AIRMAR ISO Certification (PDF Download) Supplier Change Notification (PDF Download)
Index Terms - Door Sensors - marport.com
Back to support page. Jump to index list Door Sensors
Introduction and Presentation - marport.com
Here are some examples of data received from Catch Explorer and Catch sensors displayed in Scala2. Safety Guidelines. Read this section before using the product. Description. Installation Steps. Introduction and Presentation. Read this section to get a basic knowledge of your catch sensor.