Search Results for dr otis shirley
April 4, 2013, DEPEW, NY - IMI Sensors Announces New Combustion ...
The new brochure lays out the three main applications for detecting and measuring combustion dynamics in gas turbines: Remote Sensors, Close Coupled Sensors, and On-Turbine Instability Sensors (OTIS).
Executive Leadership - Amphenol
Our leadership team remains committed to our shared responsibility of generating value for our customers, employees and shareholders while also minimizing our impact on the environment and being a positive force in our communities. Of our 22 executive leaders, six were born outside of the United States, four identify as under-represented minorities (Black or African […]
Temposonics R-Series V FLEX – Unique sensing solution for confined ...
Temposonics introduces the R-Series V FLEX, a groundbreaking position sensor that redefines flexibility and performance. Engineered for installations in confined spaces and capable of stroke lengths up to 20 meters, it is an ideal solution for demanding applications.
Acceleration Sensing Technologies for Severe Mechanical Shock - PCB
Since there is no unique definition of “severe mechanical shock,” this article first provides examples of the types of mechani-cal shock encompassed by this work. Next presented is a summary of lessons learned over the years, and pitfalls discovered, with ac-celeration sensing technologies used in past measurement attempts of these types of shock.
TPC Wire & Cable Acquires Integrated Cable Systems, Inc.
Macedonia, Ohio – February 18, 2021 - TPC Wire & Cable (TPC), a portfolio company of Audax Private Equity, announced today that it has completed the acquisition of Integrated Cable Systems, Inc. (ICS), an ISO 9001 certified supplier of custom cables, harnesses, electro-mechanical assemblies and industrial panels.
Acceleration Sensing Technologies for Severe Mechanical Shock - PCB
Since there is no unique definition of “severe mechanical shock”, this paper first provides examples of the types of mechanical shock encompassed by this work. Next presented is a summary of lessons learned over the years, and/or pitfalls discovered, with acceleration sensing technologies used in past measurement attempts of these types of shock.
SSI Technologies, LLC
We have over 25 years of experience providing magnetic sensing solutions that meet the specific needs of our OEM customers. Our line of Pressure Sensors is well suited for compact and robust sensing, while measuring pressure from 3 PSI to 7,500 PSI, and is used by top aftermarket suppliers.
Adhesive Standoff - Amphenol PCDAmphenol PCD
An elevated mounted attachment without adding holes to the structure. Made of Glass Filled Ultem and adhered using wet processes epoxy, each standoff uses 10-32 insert making it compatible with all APH Clamps; however, metric option is also available. For limited footprint, trim option also available.
More Voltage & Power - Amphenol Aerospace
We ofer high-power and high-voltage connectors with our unique power-handling technologies based around a variety of specifications, including MIL-DTL-38999, MIL-DTL-5015, MGT-5015, and more.
Switzerland - Omni Ray AG
3001 Sheldon Dr. Cary, NC, 27513. info.us@temposonics.com +1 919 677 0100 +1 800 633 7609 +1 919 677 2343; Learn more about the location; Distributor Log-In; EMEA & India Germany. Temposonics GmbH Co. KG Auf dem Schüffel 9 58513 Lüdenscheid +49 2351 9587-0 +49 2351 56491;
Staying in time – Data acquisition and transmission ... - Temposonics
In the first part of this article the data transmission via SSI as well as the asynchronous mode and the synchronous mode 1 of the R-Series V SSI were described. In this second part Dr Olaf Kissing explains the two further synchronous modes 2 and 3 of this linear position sensor.
Wilcoxon Welcomes New Director of Sales - Wilcoxon Sensing Technologies
April 11, 2022 — Frederick, MD – Wilcoxon Sensing Technologies, an Amphenol company, announces the appointment of Chris Kramm to the position of Director of Sales, responsible for leading and growing the company’s condition monitoring business.
Mounting Flange - Amphenol PCDAmphenol PCD
The Mounting flange with clinch nut works with a cylindrical square flange connector. It is ideal for rugged areas where installation and vibration is a concern. Amphenol PCD offers full, ¾ and ¼ perimeter flanges that are available with or without polyamide primer coating per MIL-PRF-23377 Type 1.
Qi2 Wireless Charging - Amphenol PCDAmphenol PCD
Amphenol PCD’s Qi2 wireless power module incorporates the latest Qi2, single coil, charging protocol with magnetic alignment, resulting in a smaller, lighter and more efficient charging surface than the previous coil Qi1X standard. As more devices move to wireless, let the latest and greatest wireless power module update your passenger experience.
News & Insights - Amphenol Ltd
• Dr Adil Imam, Senior Lecturer and Course Director of General Engineering • Dr Salman Saeidlou, Principal Lecturer and Formula Student Faculty Advisor • Tom Murphy, Christ Church Racing 2024-25 Team Captain • Adam Bayliss-Field, Christ Church Racing 2023-24 Team Captain. And from Amphenol LTD: • Ross Young, General Manager
Model 083200-01000 | PCB Piezotronics
Model 083200-01000:Model 3200 LabMaster Pro; interface w/PC via USB; w/4-channel data acquisition & signal conditioning, Analog & Digital IO for dr
Charles Universal Broadband Enclosure CUBE-PM62422MN3 and CUBE ...
LT-PM62422MN3 Page 2 of 12 6 th Printing 2. PRODUCT DESCRIPTION The CUBE has two compartments. The equipment compartment includes 24RU of 23” horizontal rack space, an 1880W DC powered heat
Rapid Part Development - Amphenol PCDAmphenol PCD
Rapid Part Development (RPD) is the ability to rapidly design and deploy production ready parts using 3D printing technology. RPD expedites part development by 86% at 1/10th the cost of standard part development cycles, providing production ready parts in 4-6 weeks. RPD uses additive-manufactured molds in the place of standard steel molds.
PCB > Learn > Videos
3425 Walden Avenue Depew, NY 14043. Sensorline SM 716.684.0001. info@pcb.com +1 800-828-8840
Charging Inlet Assembly for Aerospace ECTOL & EVTOL - Amphenol PCD
Charging Inlet Assemblies enables faster and safe DC charging for Aerospace across all regions. Includes the Combined Charging System (CCS) inlets type 1 and type 2, and North American Charging System (NACS). Each Charging Inlet Assembly can be supplied as a complete cable assembly to meet the requirements of the application.