Amphenol Socapex Introducing CTOS – The World’s Strongest Tactical Fiber Optic Connector

January 26, 2015

Dedicated to battlefield communications,  CTOS is a robust optical connector for rapid deployment of high-speed transmission links in harsh environments.

The hermaphroditic mating allows daisy chain cable assemblies without using any interconnect adapters.  CTOS is qualified by NATO according to STANAG 4290 requirements.

Main features include:

  • Expanded beam - 680 times the section of the fiber for Multimode & 5200 times the section of the fiber for Singlemode
  • Protection window - easy cleaning with a simple tissue
  • 1/2/4/8 channels
  • Stainless steel and rubber protection (10000 matting cycles)
  • Singlemode & Multimode option
  • Ethernet & RF compliant

A new section is included into the catalog presenting the Military Ethernet Media Converters equipped with CTOS. These rugged Media Converters allow to extend an Ethernet network on the field through long distance (up to 120kms).

More info on :http://www.amphenol-socapex.com/uploads/CTOS Catalog.pdf

Socapex CTOS