Amphenol Industrial Ehances AT Circular Series

September 10, 2014

Amphenol Industrial Products Group has enhanced its 9-way AT circular series receptacle line by adding one with a smaller flange so that it can be fitted to all heavy equipment vehicles. The ATC-09-9-1939PN meets SAE J1939, a specification for communication and diagnostics among industrial vehicle components.

Used as a diagnostic connector in demanding applications found on construction and farm equipment as well as in heavy-duty trucks, these round receptacles include a strain relief for the wires coming out of the back of each unit and a wave spring for higher vibration applications.

The upgraded connectors feature simple jam nut mounting for quick assembly and a smaller flange that saves space on mating panels. These corrosion resistant, heavy-duty industrial connectors are environmentally sealed against moisture and contaminants. They are water resistant up to three feet. An optional sealing cap for mating interface is available upon request.

For more information about our AT Circular Series visit Amphenol Industrial Products Group.

Press Release255.59 KB
AT-Circular-Upgrade-Web